Compact non-contact laser tool setting and tool breakage detection system for machining centres.http://www.renishaw.com/nc3
NC3 Compact non-contact laser tool setting and tool breakage detection system for machining centres. [15 kB] NCi-4 interface An NCi-4 interface is required for use with Renishaw non-contact tool setting systems. [13 kB] TJW pharmaceutical Monitoring machine capability with Renishaw’s QC10 ballbar has proved crucial to TJW, a successful machining sub-contractor who specialise in the pharmaceutical and aerospace industries. [20 kB] TJW pharmaceutical Monitoring machine capability with Renishaw’s QC10 ballbar has proved crucial to TJW, a successful machining sub-contractor who specialise in the pharmaceutical and aerospace industries. [20 kB] NCi-5 interface An NCi-5 interface is required for use with Renishaw non-contact tool setting systems. [13 kB] Machine tool probes and software Renishaw's machine tool touch probes, laser probes and software can help reduce set-up times by up to 90% and improve your process control. Key products include touch-trigger probes, machine probes, laser toolsetters, contact toolsetters, tool recognition systems, machine tool probe software and probe styli that automate part setting, fixture setting, tool setting, broken tool detection, in-cycle gauging, part verification and on-machine verification. [21 kB] Interfaces and transmission units Interfaces and transmission units A Renishaw probe must be able to communicate with the control system (CNC) of the machine on which it is fitted. Page content Downloads Call your local office Contact us online Signals must pass from the probe to the machine’s controller to register contact of the probe stylus with... [13 kB] Wireless QC20-W ballbar loses cable and gains support NC Service, a Swedish machine tool calibration and maintenance company, who work with key CNC machine users, was one of the first users worldwide to take delivery of Renishaw's QC20-W ballbar. The new design eliminates issues with the previous QC10 when used on large machines or where its data cable had to be fed through machine guarding. [18 kB] Greater process stability in large-scale manufacture Automotive component manufacturers have to guarantee consistently high machining accuracy in large batches. ZBG Zerspanungstechnik Bruck GmbH in Bruck, Oberpfalz, Germany, achieves this with the aid of the NC4 laser tool setting system from Renishaw. With this system, the machining centre checks cutting tools for wear or damage, and also determines their length to compensate automatically for any possible thermal growth of the machines in operation. [23 kB] Blog: The Prince and the Probe As mentioned in last week’s post ‘ By Royal hand `’, His Royal Highness The Duke of York opened MACH 2010 by cutting the beam of our NC4 laser tool setting system, rather than the traditional approach of cutting a ribbon. “Throw the machining rule book away and get creative” Boxtrees Precision Engineering use Renishaw probe systems on a Mazak Integrex in a clever fully-integrated ‘intelligent’ system that has achieved reduced unit costs, zero manual set-up times, unmanned machining, and consistent accuracy and cycle times [35 kB] Measuring with speed and precision A Madrid, Spain-based precision engineering business specialising in complex parts for aerospace and defence applications has invested in a Renishaw REVO® five-axis measuring head and probe system. The change has resulted in a reduction in inspection time by as much as a factor of 5, ensuring quality control and inspection keep up with its high-productivity CNC machine tools. [22 kB]
Non-contact portfolio Document comparing specifications for obsolete NC1 product and new NC3 and NC4 products. [54 kB] NC1 installation guide The NC1 system is now obsolete. Renishaw recommends upgrading your NC1 system to the NC3 or NC4 systems. [2.58 MB] NCi-4 non-contact tool setting interface data sheet The NCi-4 interface is used with Renishaws NC1, NC3 or NC4 non-contact tool setting systems. It processes signals from the non-contact unit and converts them into a voltage-free solid state relay (SSR) output, for transmission to the CNC machine control. The NCi-4 features a drip rejection mode allowing it to filter ou [388 kB] (IN414) NC Service - Wireless QC20-W ballbar loses cable and gains support Peter Jönsson, Managing Director of NC Service, Gothenburg, Sweden, has used the Renishaw QC10 ballbar (and Renishaw laser calibration systems) for years, and is convinced of the benefits, but is delighted to take delivery of the new QC20-W wireless ballbar. As he comments, “QC10 has been one of our most important tool [432 kB] Digitising introduction Overview of digitising systems and explanation of the digitising process as part of reverse engineering and re-manufacturing [8.28 MB] Renishaw introduction Introduction to the Renishaw Group, highlighting business strategy, market sectors and summarising recent innovations. [9.09 MB] Case story - NC Service - QC20-W performance testing NC Service, a Swedish machine tool calibration and maintenance company, who work with key CNC machine users, was one of the first users worldwide to take delivery of Renishaw's QC20-W ballbar. The new design eliminates issues with the previous QC10 when used on large machines or where its data cable had to be fed thro [342 kB] Case story – NC Service – QC20-W performance testing NC Service, a Swedish machine tool calibration and maintenance company, who work with key CNC machine users, was one of the first users worldwide to take delivery of Renishaw's QC20-W ballbar. The new design eliminates issues with the previous QC10 when used on large machines or where its data cable had to be fed thro [1.28 MB] NC2 software for Siemens controls The NC2 Siemens software for broken tool detection is suitable for Siemens controllers 840/810 and 802D. Please read the PDF document thoroughly for full installation details, before downloading the remaining files. [13 kB] NC2 software for NUM controls The NC2 NUM software for broken tool detection is suitable for NUM 1000 type controls (NUM 10x0 controls). Please read the PDF document thoroughly for full installation details, before downloading the remaining files. [72 kB] NC2 software for FANUC controls The NC2 Fanuc software for broken tool detection is suitable for Fanuc and Fanuc derivatives, supporting Macro B programming language and G31 skip function. Please read the PDF document thoroughly for full installation details, before downloading the remaining files. [48 kB]
NC3 coolantNC3 non-contact tool setting probe for machining centres - [100 x 100 pixels] [33 kB]
NC3 working on machineNC3 non-contact toolsetting probe for machining centres - [180 x 191 pixels] [52 kB]
- [540 x 574 pixels] [191 kB]
- [1200 x 1276 pixels] [1.42 MB]
NC3 tool setterNC3 non-contact tool setter probe for machine tools - [100 x 100 pixels] [33 kB]
NC3nc3,non-contact,tool setting - [180 x 164 pixels] [8 kB]
NC3label,interface, nc3- [180 x 273 pixels] [28 kB]
NC3interface,non-contact, nc3- [180 x 119 pixels] [10 kB]
NC3nc3,non-contact,tool setting - [540 x 493 pixels] [28 kB]
NC3nc3,non-contact,tool setting - [1200 x 1095 pixels] [186 kB]
NC3interface,non-contact, nc3- [1200 x 792 pixels] [343 kB]
NC3nc3,non-contact tool setting - [180 x 223 pixels] [7 kB]
NC3nc3,non-contact,tool setting - [1200 x 1490 pixels] [236 kB]
NC3nc3,non-contact,tool setting - [540 x 670 pixels] [22 kB]
NC3nc3,non-contact,tools setter - [540 x 348 pixels] [17 kB]
NC3nc3,non-contact,tool setter - [1200 x 773 pixels] [458 kB]
NC3nc3,non-contact,tool setting - [540 x 821 pixels] [39 kB]
NC3nc3,non-contact,tool setting - [100 x 152 pixels] [4 kB]
- [140 x 213 pixels] [6 kB]
- [200 x 304 pixels] [11 kB]
- [1200 x 1825 pixels] [589 kB]
NC3 facemill insert check An NC3 non-contact laser tool setter is used to check the condition of the inserts in a face mill. At first the tool is spun at high speed to perform a general length check. This is followed by a cycle where the tool is spun more slowly so that each insert can be checked to see that it is within a preset tolerance of [352 x 288 pixels] [0.96 MB] NC3 MicroHole video An illustration of the MicroHole™ protection system fitted to all Renishaw non-contact laser tool setting systems. A stream of coolant is prevented from entering the laser aperture by a constant stream of air. [352 x 288 pixels] [1.02 MB] NC3 tool breakage detection cycle High speed broken tool detection cycle, in which the tool is moved at rapid traverse speed to a point 0.2 mm into the beam. The tool is held in the beam for 0.1 secs, during which time the receiver checks for light receieved. If no light is received, then the tool is intact. [352 x 288 pixels] [660 kB] NC4 zoom into MicroHole The NC4's laser beam emerges through a small aperture called a MicroHole TM which, combined with a continuous air stream, protects the optics fromdebris and coolant mist. [200 x 296 pixels] [1.53 MB] NC4 rotating model Rotating exterior view of NC4 non-contact tool setter [200 x 296 pixels] [4.63 MB] NC1 broken tool check A typical broken tool detection cycle, in which the tool is quickly checked to be intact following a machining cycle. An NC1 non-contact tool setter is used to check the tool length in a simple, rapid 'plunge' check before the tool is changed. Tool breakage detection has little impact on machining cycle t [352 x 288 pixels] [1.84 MB] NC1-F face mill length & dia High speed tool setting with the NC1 non-contact laser tool setter. A face mill is set for both length and diameter, a sequence that takes less than 20 seconds to complete. A whole suite of tools can be set in just a few minutes. The sequence involves taking two readings for each dimension- the first finds [352 x 288 pixels] [3.29 MB] NC1-S slot drill length & dia This video shows a slot drill being set for length and diameter on an NC1 non-contact laser tool setter. In this installation, the transmitter and receiver units of the NC1 are mounted on bracket so that they do not intrude on the machine's operating area. Tool setting can be performed at any point along the beam. [352 x 288 pixels] [1.92 MB] NC1 through-tool coolant Many tools feature through-tool coolant to ensure optimum cutting performance. This video shows how, even with coolant pouring through the tool, Renishaw's MicroHole TM protection system and drip rejection electronics enable precise broken tool detection to be performed. [352 x 288 pixels] [1.10 MB]
|
|