Search results for Optical linear encoders
|
Page: 1 2 3 4 5 6 7 8 9
|
|
OMI optical machine interface for use with Renishaw component inspection/setting probes for machining centres and lathes. http://www.renishaw.com/omi |
|
|
|
Optical linear encoders Renishaw offers a wide range of high speed, optical linear encoder systems to meet the diverse requirements of industrial automation
| Leading encoder supplier to participate in Linear Motion Masterclass Renishaw, together with three other leading suppliers in the field of motion control, is supporting a linear motion conference organised by Eureka, a UK trade magazine for design engineers. The Linear Motion Masterclass is one of a series of the magazine’s ‘Design Days’, and takes place on 18th...
| LM10 linear magnetic encoder system New linear magnetic encoder range brings additional performance, durability and value to a wide range of applications. The LM10 linear encoder joins Renishaw’s proven family of rotary magnetic encoders. The new LM10 linear magnetic encoder brings 100 m travel and fit-and-forget reliability to...
| Welcome to Renishaw In metrology, motion control, machine calibration, dental CAD/CAM and spectroscopy, Renishaw innovations enhance precision, efficiency and quality.
| TONiC™ RGSZ linear encoder TONiC RGSZ gold tape scale linear encoder. Home. Position encoders. Optical linear encoders. TONiC RGSZ linear encoder. TONiC T1000 series represents a new generation of super-compact encoders, specially designed for highly-dynamic precision linear motion systems, bringing higher accuracy,...
| RG2 optical linear encoder The RG2 is an open, non-contact optical linear encoder system, eliminating friction and wear whilst permitting reliable high speed, high resolution operation. The unique 20 µm pitch optics ensure excellent signal stability in conditions considered unsuitable for most open optical linear encoders.
| Measurement optics Renishaw measurement optics enable you to measure linear, pitch, yaw, horizontal and vertical straightness along any axis. Additional optic kits are available to enable measurement of surface flatness and squareness of axis.
| RG4 optical linear encoder The RG4 open, non-contact optical linear encoder system eliminates friction and wear whilst permitting reliable high speed, high resolution operation. The 40 µm scale pitch allows higher speeds and greater set-up tolerances. In addition, RG4 systems are able to read a wider variety of scale types.
| OMI-2 / OMI-2C A combined optical receiver/interface, which conveys and processes signals between an inspection probe and the CNC machine's control.
| Magnetic linear encoders The LM10 linear magnetic encoder features a compact sealed readhead that rides at up to 1.5 mm from the self-adhesive magnetic strip scale, with up to 100 m travel.
| TONiC™ RSLM encoder system TONiC RSLM stainless steel linear encoder system. Home. Position encoders. Optical linear encoders. TONiC RSLM encoder system. The new RSLM stainless steel spar scale offers performance to rival fine pitch glass scales yet is available in lengths up to 5 m. RSLM offers a total accuracy...
| RGH34 encoder system The open, non-contact RGH34 encoder is a versatile miniaturised component system. Designed for OEM applications where a conventional enclosed readhead cannot be fitted, the RGH34 brings reliable performance to compact precision linear actuators, microscopes, and microstages.
| OMP60 Touch probe with optical transmission suitable for component inspection and set-up on medium to large machining and mill-turn centres.
| Laser10 software The user interface to the ML10 Gold Standard laser system
| TONiC™ RELM encoder system TONiC RELM high accuracy linear encoder system. Home. Position encoders. Optical linear encoders. TONiC RELM encoder system. The RELM high accuracy scale offers high speed, non-contact performance, combined with advanced features including dynamic signal processing and the IN-TRAC auto-phase optical
| MP10 Compact optical transmission inspection probe for machining centres, now superseded by OMP60.
| Optics A number of optical accessories are available to ease set-up, alignment and operation of your Renishaw laser measurement system.
| Renishaw on high with Airbus A380 Superjumbo Home. Corporate. News. Encoders for motion control. A380 panel assembly. Renishaw on high with Airbus A380 Superjumbo. By virtually every measure of comparison, the new Airbus A380 Superjumbo, now under final construction in Europe, is the largest commercial aircraft in the world. Able to...
| MP8 Shank-switch operated touch trigger inspection probe system with optical transmission for machining centres.
| OTS OTS cableless optical tool setting and broken tool detection for vertical machining centres.
|
| Page: 1 2 3 4 5 6 7 8 9 |
|
Page: 1 2 3 4
|
 | RELM/RELE installation drawing RELM/RELE installation drawing [144 k]
|  | New encoder software eases motion system set-up, calibration and diagnostics A powerful component of Renishaw's new SiGNUM family of angle and linear encoders is the PC-based SiGNUM software that provides comprehensive calibration, set-up optimisation and real-time diagnostics. [52.2 k]
|  | SiGNUM software SiGNUM software sales flyer [555 k]
|  | Renishaw on high with Airbus A380 Superjumbo - News article By virtually every measure of comparison, the new Airbus A380 Superjumbo, now under final construction in Europe, is the largest commercial aircraft in the world. Able to accommodate 555 passengers, and with a wingspan in excess of 260 feet, building the giant double-decker calls for some... [26 k]
|  | TONiC™ encoder news release - text only - News article New super-compact optical encoder offers speed, accuracy and reliability [136 k]
|  | LM10 linear magnetic encoder - text only Text only news release about Renishaw's LM10 linear magnetic encoder [30.5 k]
|  | SiGNUM™ RSLM high accuracy stainless steel scale data sheet - Data sheet [210 k]
|  | RSLM - News article [27.5 k]
|  | Product release - World’s first 13-bit magnetic rotary encoder - News article Renishaw offers a wide range of magnetic and compact optical position feedback encoder systems to meet the diverse requirements of industrial automation. The latest additions to the range include the world’s first 13-bit magnetic sensor, which is sealed for operation in harsh environments,... [27.5 k]
|  | MYDATA take a different approach to the design of large-board SMT machines - News article MYDATA is one of the world’s leading developers and suppliers of pick and place machines for the electronic industry, set apart from other manufacturers by the flexibility and fast change-over their machines offer. Its new generation of large-board machines has broken new ground, with recently... [28 k]
|  | Ultra-accurate lends measuring systems features advanced air bearing and encoder technologies - News article [94.5 k]
|  | Twin probe system - news release - text only - News article Renishaw’s new twin probe optical signal transmission system uses a single optical receiver for tool setting probe and spindle mounted touch probe installations, offering fast integration and a cable-free machine environment. [28 k]
|  | Renishaw introduction Introduction to the Renishaw Group, highlighting business strategy, market sectors and summarising recent innovations. [9.09 M]
|  | Renishaw at MSV Brno 2008 news release - text only - News article Renishaw is focusing on speed of manufacture at MSV Brno, with new products that will help businesses to manufacture profitably, by reducing process times and minimising the cost of poor quality for a wide range of machining and measurement applications. The MSV Brno show takes place at the Brno... [29 k]
|  | Laser calibration system spot on - News article Inca Digital Printers has developed the first ever flatbed inkjet press, which looks set to revolutionise a major sector of the screen print market. Such hi-tech printing equipment demands advanced manufacturing techniques to ensure supreme accuracy, which in this case is provided by Renishaw... [26 k]
|  | SiGNUM™ FANUC news release - text only - News article [27.5 k]
|  | New encoder catalogue includes high accuracy linear scale and magnetic rotary encoders Renishaw offers a wide range of compact optical and magnetic encoder systems to meet the diverse requirements of industrial automation. The company's latest encoder product catalogue features Renishaw's full range of linear, angle, magnetic encoders and laser interferometers [68.3 k]
|  | The need for speed - Renishaw at JIMTOF 2008 news release - News article Renishaw is focusing on speed of manufacture at JIMTOF 2008, with a range of new products that will help businesses to manufacture profitably, by reducing process times and minimising the cost of poor quality for a wide range of machining and measurement applications. The JIMTOF 2008 show takes... [31 k]
|  | Renishaw opens new Indian training and demonstration centre - text only - News article World leading measurement company Renishaw, opened its first dedicated demonstration and training centre for the Indian market at its main office in Pune on January 17th 2008. [137 k]
|  | Laser step diagonal tests - There are some fundamental flaws in the laser step diagonal or vector me Laser step diagonal tests
There are some fundamental flaws in the laser step diagonal or vector measurement method.
<br><br>
The method cannot be used to reliably determine the linear positioning errors in a machine and should not be used for linear error compensation of a machine. Even though... [716 k]
|
|
Page: 1 2 3 4
|
|
|
|
Personalisation
Recent searches
Log in to show recent searches
|