High performance encoders for military and aerospace High performance encoders for military and aerospace High performance position encoders for mission critical reliability. Suitable for use in demanding applications such as targeting systems, remotely-operated weapons, long range vision systems and radar installations. Page content Downloads Call your local office... [23 kB] Upgraded machine tool performance monitoring device receives worldwide acclaim Upgraded machine tool performance monitoring device receives worldwide acclaim. Launched in November 2009, Renishaw's QC20-W telescoping ballbar which incorporates Bluetooth® wireless technology has had a significant impact on CNC machine testing around the world. Many customers have found that that the new QC20-W ballbar offers significant advantages over Renishaw’s QC10 product, which was for many years the industry standard test for machine tool performance. [20 kB] Renishaw supports new US HTEC centre with performance testing tool Haas, one of the world’s leading machine tool manufacturers, has boosted its Haas Technical Education Centre (HTEC) programme in the USA, with the opening of a dedicated HTEC teacher training centre at Vincennes University (VU), Indiana. To support the new facility, Renishaw, a long-term HTEC industrial partner, has donated a QC20-W wireless ballbar, which will be used to help train users of the new centre in the importance of regular machine tool performance testing. [16 kB] Performance and testing All of Renishaw's experience in metrology and laser interferometry is to be found in each and every measurement system that it produces. Our aim is to deliver the specified accuracy, with full traceability and confidence that the laser system will continuously deliver that accuracy day-after-day where it counts, in the workplace. [15 kB] RLE20 interferometer enhances performance of Vistec Lithography’s latest e-beam tool Vistec Lithography’s (previously Leica Microsystems) VB300 e-beam lithography tool is a development of the highly successful VB6 series introduced in 1993. In designing the new tool, Vistec identified that a reduction of noise-induced positional errors would significantly improve tool performance. Through a combination of improved mechanical rigidity and integration of the Renishaw RLE20 differential interferometer based encoder system, these errors are now expected to be 3 nm. [28 kB] Improved measurement performance with new motorised heads for co-ordinate measuring machines Following a series of design enhancements, Renishaw’s industry-standard family of PH10 motorised indexing heads for co-ordinate measuring machines (CMMs) now have a 20% improvement in repeatability and increased long-term stability. Combined with an optional extended 2-year warranty, the new PH10 heads offer CMM users a new standard of indexing head performance, providing reliable precision in even the most demanding measurement applications. [19 kB] RESOLUTE™ absolute optical encoder - Performance Renishaw is introducing RESOLUTE, a true absolute, fine pitch optical encoder system that has excellent dirt immunity, and an impressive specification that breaks new ground in position feedback. [41 kB] ‘Consistently high performance’ earns Renishaw another Queen’s Award for Enterprise On Wednesday 20th July, Renishaw plc was presented with a Queen’s Award for Enterprise 2011 by Dame Janet Trotter, Her Majesty’s Lord-Lieutenant of Gloucestershire. This is Renishaw’s fourteenth Queen’s Award since its formation in 1973, and was granted in the Innovations category for the company’s TRS2 laser-based non-contact broken tool detection system. [15 kB]
RLE system performance data sheet Data sheet describes the RLE system which provides the positioning performance expected from an interferometer, with ease of installation and use. [1.65 MB] SP600 family Overview of the SP600 range of high performance scanning probes, covering applications, design features and performance specification [7.75 MB] SP25M compact scanning probe The SP25M is the world's most compact and versatile scanning probe. This presentation provides a description of the benefits, key design features, performance of the SP25M, plus ordering information. [9.06 MB] PH10 family Overview of the PH10 range of indexing heads, covering applications, key design features and performance [7.46 MB] Attacking waste Public enemy #1: non-value added activities that consume time and resources [2.61 MB]
ML10 Gold StandardImproved machine accuracy for better measurement, machining or processing performance. Phase Motion Control SrlItalian company specilising in high torque direct drives, high performance electric linear actuators and drives for electric traction. Site includes product descriptions, contact information and a description of the company. - [180 x 100 pixels] [11 kB]
ML10 Gold Standard laserML10 Gold St andard laser - The ultimate in precision machine performance measurement and calibration. - [100 x 112 pixels] [10 kB]
QC20-W wireless ballbar set-up The QC20-W telescoping ballbar provides a simple, rapid check of a CNC machine tool's positioning performance to recognised international standards (e.g. ISO, ASME etc) allowing users to benchmark and track the performance of their machines and to quickly diagnose problems that require maintenance. [640 x 360 pixels] [4.50 MB], [720 x 576 pixels] [32.59 MB] NC1 through-tool coolant Many tools feature through-tool coolant to ensure optimum cutting performance. This video shows how, even with coolant pouring through the tool, Renishaw's MicroHole TM protection system and drip rejection electronics enable precise broken tool detection to be performed. [352 x 288 pixels] [1.10 MB]
|
|