Search results for RGH40 encoder system
|
Page: 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18
|
|
The open, non-contact RGH40 readhead is designed for use with Renishaw's 40 µm RGS40-G glass scale or 40 µm RESR ring and offers resolutions to 50 nm. http://www.renishaw.com/rgh40 |
|
|
|
RGH40 encoder system The open, non-contact RGH40 readhead is designed for use with Renishaw's 40 µm RGS40-G glass scale or 40 µm RESR ring and offers resolutions to 50 nm.
| RG4 optical linear encoder The RG4 open, non-contact optical linear encoder system eliminates friction and wear whilst permitting reliable high speed, high resolution operation. The 40 µm scale pitch allows higher speeds and greater set-up tolerances. In addition, RG4 systems are able to read a wider variety of scale types.
| RESR angle encoder system Renishaw's RESR angle encoder offers impressive performance. With graduation accuracy to ±0.5 arc second and resolution to 0.01 arc second, the RESR suits the most demanding precision applications.
| TONiC™ RESM angle encoder system angle compact encoder resm ring rotary system tonic. Home. Position encoders. Optical angle encoders. TONiC RESM angle encoder system. RESM angle encoder offers accuracy, resolution, and repeatability at high speed and high temperature. It also offers ultra-low cyclic error and the IN-TRAC...
| SiGNUM™ RSLM encoder system The new RSLM stainless steel spar scale offers performance to rival fine pitch glass scales yet is available in lengths up to 5 m. RSLM offers a total accuracy (including slope and linearity) better than ±4 μm over 5 m – an industry first! With ±30 nm cyclic error, patented filtering optics,...
| TRS1 TRS1 single-sided non-contact broken tool detection unit for machining centres
| Flying success with Dunlop Aerospace Braking Systems Renishaw probes cut production time
| SiGNUM™ RESM angle encoder system SiGNUM™ RESM angle encoder offers accuracy, resolution, and repeatability at high speed and high temperature. It also offers ultra-low cyclic error and the IN-TRAC™ optical reference mark. The RESM angle encoder offers performance to suit the most demanding precision applications.
| Encoder comparison table Please use the tables below to compare Renishaw's range of optical linear and optical angle encoder systems. For further information and product options, please visit the encoder product configurator.
| Renishaw wins two prestigious awards at leading international event At the prestigious MWP Awards Dinner held in Birmingham, UK, on 22nd April, Renishaw plc was honoured with two awards for product excellence. The awards, which are often referred to as the UK metalworking industry’s ‘Oscars’, were achieved against strong competition, with entry open to any...
| MP10 Compact optical transmission inspection probe for machining centres, now superseded by OMP60.
| PHS1 servo head PHS1 servo positioning head provides full servo control in two rotary axes, allowing the probe to be positioned in almost any orientation.
| Twin probe system The Renishaw twin probe system allows a spindle probe and a tool setting probe to be installed on a machine with a single optical interface.
| New super-compact optical encoder offers speed, accuracy and reliability TONiC™ is Renishaw's latest super-compact optical encoder, offering exceptional performance and versatility with refreshing simplicity.
| RGH25 encoder system The open, non-contact and ultra-compact RGH25 readhead uses Renishaw's unique flexible 20 µm RGS20-S tape scale and offers resolutions to 10 nm. The low profile RGH25 features external interpolation through a range of interfaces, which offer automatic gain control, offset control, and diagnostic...
| TONiC™ angle compact encoder linear optical rotary small systems tonic. Home. Position encoders. Optical linear encoders. TONiC. TONiC is Renishaw’s new super-compact non-contact optical encoder that offers speeds up to 10 m/s and resolutions down to 5 nm for both linear and rotary applications. Offerin
| SiGNUM™ RSLM high accuracy stainless steel scale With ±30 nm cyclic error, patented filtering optics, resolution to 5 nm and simple installation, Renishaw's SiGNUM™ RSLM encoder system provides all of the benefits of a 20 μm encoder with the performance of a fine pitch system.
| TONiC™ RSLM encoder system TONiC RSLM stainless steel linear encoder system. Home. Position encoders. Optical linear encoders. TONiC RSLM encoder system. The new RSLM stainless steel spar scale offers performance to rival fine pitch glass scales yet is available in lengths up to 5 m. RSLM offers a total accuracy...
| SPA2 Home. CMM. Controllers. SPA2. The SPA2 is a 4-channel digital servo power amplifier with an integral power supply.About SPA2-2. SPA2-2 has been optimised to work with the. UCC2. CMM controller and. MCU1. joystick, together forming an ideal retrofit package.. Key features:. For each amplifier channe
| FAQs FAQs - product support questions associated with Renishaw's RLE laser interferometer-based position feedback system
|
| Page: 1 2 3 4 5 6 7 8 9 10 11 12 13 14 15 16 17 18 |
|
Page: 1 2 3 4 5
|
 | Laser calibration system spot on - News article Inca Digital Printers has developed the first ever flatbed inkjet press, which looks set to revolutionise a major sector of the screen print market. Such hi-tech printing equipment demands advanced manufacturing techniques to ensure supreme accuracy, which in this case is provided by Renishaw... [26 k]
|  | RSLM - News article [27.5 k]
|  | Renishaw on high with Airbus A380 Superjumbo - News article By virtually every measure of comparison, the new Airbus A380 Superjumbo, now under final construction in Europe, is the largest commercial aircraft in the world. Able to accommodate 555 passengers, and with a wingspan in excess of 260 feet, building the giant double-decker calls for some... [26 k]
|  | Product release - World’s first 13-bit magnetic rotary encoder - News article Renishaw offers a wide range of magnetic and compact optical position feedback encoder systems to meet the diverse requirements of industrial automation. The latest additions to the range include the world’s first 13-bit magnetic sensor, which is sealed for operation in harsh environments,... [27.5 k]
|  | TONiC™ encoder news release - text only - News article New super-compact optical encoder offers speed, accuracy and reliability [136 k]
|  | Renishaw opens new Indian training and demonstration centre - text only - News article World leading measurement company Renishaw, opened its first dedicated demonstration and training centre for the Indian market at its main office in Pune on January 17th 2008. [137 k]
|  | LM10 linear magnetic encoder - text only Text only news release about Renishaw's LM10 linear magnetic encoder [30.5 k]
|  | SiGNUM™ FANUC news release - text only - News article [27.5 k]
|  | Ultra-accurate lends measuring systems features advanced air bearing and encoder technologies - News article [94.5 k]
|  | Renishaw at MACH 2008 - text only - News article Renishaw is focusing on speed of manufacture at MACH 2008, with new products and training initiatives that will help businesses to manufacture profitably within the UK, by reducing process times and minimising the cost of poor quality for a wide range of machining and measurement applications. [27.5 k]
|  | RLE20 interferometer enhances performance of Vistec Lithography’s latest e-beam tool - News article Vistec Lithography’s (previously Leica Microsystems) VB300 e-beam lithography tool is a development of the highly successful VB6 series introduced in 1993. In designing the new tool, Vistec identified that a reduction of noise-induced positional errors would significantly improve tool... [33.5 k]
|  | New General Manager for Renishaw’s Swedish subsidiary - News article World leading technology company Renishaw has appointed a leading figure from the Swedish metrology industry to head up its Nordic operations. Bo Eneholm, aged 42, was until recently General Manager of Hexagon Metrology’s Nordic office, and as well as a deep knowledge of measurement... [136 k]
|  | Laser calibration reduces costs and gives four-fold accuracy improvement for CNC water-jet cutting machine manufacturer - News article Czech manufacturer PTV, spol s.r.o., based in Prague, has experienced a very rapid increase in sales of its CNC water-jet cutting machines. To help manage this growth, the company uses Renishaw’s ML10 laser interferometer measurement system and QC10 ballbar, which has reduced manufacturing... [31 k]
|  | Flying success with Dunlop Aerospace Braking Systems - text only - News article Case story – MT part set-up - Flying success with Dunlop Aerospace Braking Systems - Renishaw probes cut production time [29 k]
|  | Renishaw to speak at UK and India conference - text only - News article World leading measurement company Renishaw plc has been invited by the UK Government’s Trade & Investment organisation (UKTI) to speak about its experiences of investing in India at the Advanced Engineering Summit taking place
in New Delhi, India on Tuesday, 15th January 2008. [136 k]
|  | Renishaw highlights the need for speed at Control 2008 - text only - News article Renishaw is focusing on speed of measurement and manufacture at Control 2008, with products that will help businesses to manufacture profitably, by reducing process times and minimising the cost of poor quality for a wide range of machining and measurement applications. [30.5 k]
|  | NC4 non-contact tool setter Explanation of the benefits and key features - MicroHole<sup>TM</sup> and PassiveSeal<sup>TM</sup> - of the NC4 non-contact tool setting and broken tool detection system. [801 k]
|  | Renishaw introduction Introduction to the Renishaw Group, highlighting business strategy, market sectors and summarising recent innovations. [9.09 M]
|  | Air bearing production given a lift - News article The rise in the popularity of air bearing spindles for new applications owes much to the ability of modern machine tools to provide extremely tight dimensional tolerances and fine surface finishes. Achieving such results, however, can involve lengthy set-up times; especially where batch... [26.5 k]
|  | ZBG case story - Greater process stability in large-scale manufacture - text only - News article Automotive component manufacturers have to guarantee consistently high machining accuracy in large batches. ZBG Zerspanungstechnik Bruck GmbH in Bruck, Oberpfalz, Germany, achieves this with the aid of the NC4 laser tool setting system from Renishaw. With this system, the machining centre... [93 k]
|
|
Page: 1 2 3 4 5
|
|
|
| No other media match your search terms. |
|
|
|
|
|
Personalisation
Recent searches
Log in to show recent searches
|