|
22 results found.
|
双测头系统 The Renishaw twin probe system allows a spindle probe and a tool setting probe to be installed on a machine with a single optical interface. [8 kB] OMI-2H Combined optical transceiver/interface, which conveys and processes signals for two different probes sequentially. [7 kB] 加工中心用工件检测软件 Inspection macro software for Renishaw component setting and inspection probes for machining and turning centres. [7 kB] OMI-2T Combined optical transceiver/interface, which conveys and processes signals for two different probes sequentially. [8 kB] Active Editor Pro Productivity+™ Active Editor Pro is the all-in-one solution for producing probing cycles remotely from the machine, via a CAD interface. [12 kB] Air bearing production given a lift Air bearing production given a lift 目前本页还没有简体中文版。您可以使用Google的翻译服务查阅 自动翻译 。我们不负责提供该项服务,而且翻译结果未经过我们的检查。 如果您需要更多帮助,请 联络我们 。 The rise in the popularity of air bearing spindles for new applications owes much to the ability of modern machine tools to provide extremely tight dimensional tolerances and... [10 kB] MP700高精度接触式测头 Spindle mounted optical transmission measurement probe with superior 3D performance. [13 kB] TJW pharmaceutical Monitoring machine capability with Renishaw’s QC10 ballbar has proved crucial to TJW, a successful machining sub-contractor who specialise in the pharmaceutical and aerospace industries. [13 kB] TJW制药 Monitoring machine capability with Renishaw’s QC10 ballbar has proved crucial to TJW, a successful machining sub-contractor who specialise in the pharmaceutical and aerospace industries. [13 kB] Renishaw at EMO 2007 Renishaw focused on speed of manufacture at EMO 2007 (September 2007, in Hannover, Germany), with a range of new products that help businesses to reduce process times whilst maintaining quality in a wide range of machining and measurement applications. [9 kB] 追求高精高速 Renishaw is focusing on speed of manufacture at MSV Brno, with new products that will help businesses to manufacture profitably, by reducing process times and minimising the cost of poor quality for a wide range of machining and measurement applications. The MSV Brno show takes place at the Brno exhibition centre from 15th to 19th September and Renishaw’s stand is located in Pavilion V stand 65. [9 kB] RLP40紧凑型测头 RLP40 pioneers the application of frequency hopping spread spectrum (FHSS) radio transmission in the turning centre environment. Where line-of-sight between an optical inspection probe and interface cannot always be maintained the application of the RLP40 with an RMI interface unit maintains reliable communications. [13 kB] OLP40紧凑型测头 OLP40 is Renishaw’s smallest inspection probe with optical signal transmission for lathe and turning centres, using Renishaw’s well established optical interfaces. The OLP40 can use Renishaw’s legacy or modulated optical signal
transmission systems without any compromise in metrology performance.
When used with an OMI-2T interface unit, two OLP40s can be used on the same machining centre. [13 kB] RMP60接触式测头 A touch-trigger probe with radio transmission method for component setting/inspection on machining centres. [14 kB] MACH 2008:追求高速高精 Renishaw is focusing on speed of measurement and manufacture at MACH 2008 (Hall 5 Stand 5140), with products that will help businesses to manufacture profitably, by reducing process times and minimising the cost of poor quality for a wide range of machining and measurement applications. [12 kB]
Lathe set upLathe set-up with Renishaw machine tool probes for on- machine inspection, component and tool setting. - [100 x 100 pixels] [8 kB]
|
|