|
361 results found.
|
QC10系统软件 QC10球杆仪可以采集数据,而Ballbar 5软件则为用户提供更有价值的信息。Ballbar 5软件包与Windows®兼容,可对机床性能进行分析。 与QC10球杆仪一样,Ballbar 5软件功能强大,使用方便。 Windows界面和循序渐进的操作说明意味着您在几分钟之内就可以使用系统。 [18 kB] QC10球杆仪系统 QC10球杆仪系统 网页内容 下载 致电当地的办事处 在线联系我们 自动1991年以来,Renishaw的QC10伸缩式球杆仪已被公为为最佳、最实用的快速评估机床综合位置性能的方法。 如今,它已被全球数以千计的用户广泛采用,用户群包括最大的机床制造商、最终用户和服务公司。 自2009年10月起,QC10球杆仪系统将被 QC20-W无线球杆仪系统 正式取代。 QC10支持 Renishaw承诺一如既往地为所有QC10系统用户提供支持。 我们将按照既定政策继续为所有QC10球杆仪提供若干年的全面服务、重新校准及维修(包括工厂保修的换修装置)。... [12 kB] Ballbar gives significant time savings for lathe manufacturer Binns & Berry is one of the few remaining family-owned machine tool manufacturing companies in the UK. It manufactures CNC lathes to individual customer specifications as well as providing a refurbishment service for existing machines. The company is renowned for its large, rigid machines, supplied with axis swings of between 0.7m and 1.4m. Currently, over half of the company’s business is exported, with major markets including the USA, India, Germany and Hong Kong. [15 kB] 产品支持和培训 Renishaw sales engineers are renowned for their pre and post sales support. We know that buying a laser system is a major investment for you and your company. Please ask us if you have any questions, we’ve nothing to hide and we want you to be sure you choose the right solution for your application. [12 kB] Scania - 机床维护是投资不是成本! Scania - 机床维护是投资不是成本! 网页内容 下载 致电当地的办事处 在线联系我们 Dynamate AB是为世界领先的卡车制造商Scania公司提供设备维护的公司。它实施了一套堪称业内最全面、结构最合理的维护方案。这套方案的核心是,利用Renishaw的QC10球杆仪系统来监控500多台大型数控机床的性能。 Dynamate的方案为Scania设在斯德哥尔摩附近的Södertälje加工厂带来巨大的变化,并被证明具有重大意义:机床精度和机床生产能力都获得大幅提高,从而能加工出高质量的零件。其中最重要的是,充分认识到了以标准化测试程序定期监控机床性能的重要性。... [17 kB] 支持QC10的附件 采用以下附件可以增强QC10系统的功能: 校准规、360°车床适配器、小圆组件、VTL适配器。 [12 kB] QC10组件 The ballbar kit is presented in a handy carry case, including everything needed for most machining centre tests. You just need to add a PC to start testing. [6 kB] QC20-W球杆仪系统 QC20-W球杆仪系统 网页内容 下载 致电当地的办事处 在线联系我们 采用新型QC20-W球杆仪系统,伸缩式球杆仪测试变得更为简单,功能更强大。 QC20-W系统是基于Renishaw多年球杆仪测试的经验而推出的,与已有的QC10系统相比,性能更优异,操作优点更显著。 蓝牙 (Bluetooth) 无线技术确保了无需处理线缆问题、在防护门关闭的状态下操作,并降低了系统损坏的可能性。 新硬件和软件允许您进行“部分圆弧”(220°) 测试。 测试的灵活性获得提高,包括: Z轴测试获得提高(无需用户定制卡具) 降低了轴行程的要求(典型情况下,加工中心的Z轴和车床的X轴)... [15 kB] QC20-W球杆仪系统软件 QC20-W球杆仪系统软件 网页内容 下载 致电当地的办事处 在线联系我们 Ballbar 20是基于技术成熟的Ballbar 5软件开发的,对QC10和QC20-W球杆仪系统都适用。 除了支持 '360°' 测试程序的已有功能及增强功能外,它还支持用QC20-W(及合适的硬件)进行220°“部分圆弧”测试和全新的“空间诊断”功能。 新特性: Ballbar 20 Ballbar 20软件是为QC20-W无线球杆仪系统开发的。这意味着即使您同时使用QC10和QC20-W球杆仪,也可以运行单个软件程序。如果您目前只有一套QC10,为何不升级,充分利用Ballbar 20的许多新增功能呢?... [18 kB] QC10 ballbar a key quality and productivity tool in Rockwell Automation's Power Lean manufacturing QC10 ballbar used for both diagnosis and predictive maintenance to keep machine tools running and producing to specification. Rockwell Automation Power Systems specialises in providing technologies and services for optimising power transmission performance and productivity. The company has turned its analytical and creative skills to developing an integrated process for continuous improvement of the manufacturing processes in its own plants. [20 kB] QC20-W球杆仪附件 采用以下附件可以增强QC20-W系统的功能: 校准规、360°车床适配器、小圆组件、VTL适配器。 [11 kB] 测试理论及实践 测试理论及实践 网页内容 下载 致电当地的办事处 在线联系我们 球杆仪测试之所以广受欢迎,缘于测试本身简单易行、设定简单、使用便捷,而且测试报告可向操作者提供大量有用信息。 现在,您可以看到Renishaw如何将这些特性融入QC20-W,提供更多的功能和更简单的测试程序。 测试原理是什么? 理论上,如果在数控机床上编程跟踪圆轨迹而且机器定位性能为理想状态,则实际圆会与设定圆吻合。在实践中,机器几何尺寸中的很多因素、控制系统及磨损都可能造成测试圆半径及其形状偏离设定圆。 如果您能精确测量实际的圆轨迹,并将其与设定轨迹进行比较,则将获得机器精度的测量值。... [17 kB] 伸缩式球杆仪系统 伸缩式球杆仪系统 网页内容 下载 致电当地的办事处 在线联系我们 今天,有一种仪器被全球公认为最实用、最方便和测试内容最全面的评估数控机床轮廓精度的工具,那就是伸缩式球杆仪。 请不要将这种伸缩式球杆仪与用于坐标测量机 (CMM) 校准的固定长度的空间精度校准规相混淆。它按照公认的国际标准(如ISO、ASME等)对数控机床的定位性能进行简单、快捷的检测,允许用户对机床性能进行基准测试及追踪机床性能,并在需要维护时快速诊断出机床存在的问题。 对机床定期进行球杆仪测试有助于 确保数控机床一次性加工出合格零件 减少机床停机时间、降低废品率和检测成本... [16 kB] 质量 Many Renishaw users worldwide can testify to the performance and reliability in use of their Renishaw lasers and QC10 ballbars. The performance has been verified by national standards laboratories over many years and reliability is seen by users who find that systems operate ¢out of box¢ and continue to do so with minimal repairs over the years. [11 kB]
新闻文章:Renishaw QC20-W球杆仪 — 具有空间测试能力的新型无线产品 Renishaw宣布继信誉良好的QC10球杆仪系统之后推出新一代产品。QC10球杆仪在全球广泛应用于机床定位和伺服控制性能评估。 QC20-W球杆仪采用Renishaw全新设计、开发的直线位移传感器和蓝牙 (Bluetooth™) 无线技术。这种设计具有使用方便和耐用性强的优点,从而使QC20-W可用于“防护门关闭”状态下进行测试,此前同类有连线的系统需在“防护门开启”状态下测试,可能造成安全和程序上的问题。 [147 kB] 案例分析 — Scania — 机床维护是投资不是成本! Dynamate AB是为世界领先的卡车制造商Scania公司提供设备维护的公司。它实施了一套堪称业内最全面、结构最合理的维护方案。这套方案的核心是,利用Renishaw的QC10球杆仪系统来监控500多台大型数控机床的性能。 [32 kB] 新闻文章 - XL-80全新轻巧型激光干涉仪测量系统:便携性强、高性能、使用方便 你只要看一眼Renishaw的新型XL-80激光系统和XC-80补偿器,就会注意到它们比原有的ML10和EC10小了许多。现在,二者总重仅3公斤多一点(包括连接电缆、电源和传感器),比原来减轻了70%。当然,随着激光头和补偿器尺寸减小,其他系统组件,例如三脚架和云台也相应地减小以便相配,因此整个系统(配小型三脚架)的运输箱减小了许多。现在,最小的“脚轮箱”只有原来箱子的一半大一点,却可以携带整个线性和角度测量系统,并按需预留放置Renishaw QC10球杆仪组件的位置。这个高度便携的“检查和修正”激光干涉仪和球杆仪组合系统总重不到17公斤,令同类产品无以匹敌。 [48 kB] 案例分析 — Renishaw的机床检测工具为Haas立式加工中心优化精度 Haas自动化公司过去在其每一台VF立式加工中心上都进行机械式纵向负载测试,然后将测得结果输入CNC作为补偿值,以对每台机床的精度进行精调。然而,最近他们在此基础上又增加了一个检测项目,即使用Renishaw QC10球杆仪进行反向间隙补偿。通过检测在一个整圆上的位置误差,球杆仪可以提取出一些经常被传统机械检测所忽视的结果,包括摩擦力的影响和电机与滚珠丝杠连接的问题。 [27 kB] 新闻文章 - XL-80全新轻巧型激光干涉仪测量系统:便携性强、高性能、使用方便 你只要看一眼Renishaw的新型XL-80激光系统和XC-80补偿器,就会注意到它们比原有的ML10和EC10小了许多。现在,二者总重仅3公斤多一点(包括连接电缆、电源和传感器),比原来减轻了70%。当然,随着激光头和补偿器尺寸减小,其他系统组件,例如三脚架和云台也相应地减小以便相配,因此整个系统(配小型三脚架)的运输箱减小了许多。现在,最小的“脚轮箱”只有原来箱子的一半大一点,却可以携带整个线性和角度测量系统,并按需预留放置Renishaw QC10球杆仪组件的位置。这个高度便携的“检查和修正”激光干涉仪和球杆仪组合系统总重不到17公斤,令同类产品无以匹敌。 [361 kB]
QC10 ballbarQC10 ballbar - szybkie testowanie stanu technicznego obrabiarek - [270 x 170 pixels] [13 kB]
QC10 ballbarQC10 ballbar - [220 x 55 pixels] [2 kB]
- [360 x 89 pixels] [5 kB]
- [1200 x 298 pixels] [90 kB]
QC10 ballbarQC10 automated ballbar used by Zeeco to run dynamic tests on 2 axes at a time, in this case the Y and Z axes, to measure any deviations from a - [180 x 135 pixels] [9 kB]
- [540 x 405 pixels] [23 kB]
- [2400 x 1800 pixels] [2.05 MB]
QC10 ballbar on machine tool bedQC10 ballbar on machine tool bed - [180 x 137 pixels] [4 kB]
- [200 x 153 pixels] [46 kB]
- [540 x 412 pixels] [119 kB]
- [1200 x 916 pixels] [64 kB]
- [1772 x 1353 pixels] [673 kB]
キャリブレータ熱膨張がほとんどない特許材から作られたこの基準球を使用することで、使用前に QC10 を較正でき、絶対計測値を取得できます。 (例えば、軸間のスケールミスマッチだけでなく、軸上のスケール誤差を確認できます。) - [100 x 58 pixels] [2 kB]
- [180 x 104 pixels] [4 kB]
QC10 ballbar- [80 x 85 pixels] [2 kB]
- [100 x 106 pixels] [2 kB]
- [120 x 127 pixels] [2 kB]
- [180 x 191 pixels] [4 kB]
- [220 x 234 pixels] [5 kB]
- [500 x 531 pixels] [90 kB]
Haas case study imageQC10 ballbar testing positioning performance on a HAAS VMC - [180 x 135 pixels] [6 kB]
- [1200 x 900 pixels] [76 kB]
QC20-W partial arc 480x272 Partial arc test with QC20-W [480 x 272 pixels] [7.35 MB], [640 x 360 pixels] [3.79 MB], [640 x 360 pixels] [10.72 MB], [1280 x 720 pixels] [13.52 MB] QC20-W wireless ballbar set-up The QC20-W telescoping ballbar provides a simple, rapid check of a CNC machine tool's positioning performance to recognised international standards (e.g. ISO, ASME etc) allowing users to benchmark and track the performance of their machines and to quickly diagnose problems that require maintenance. [640 x 360 pixels] [4.50 MB], [720 x 576 pixels] [32.59 MB] QC20-W standard test standard 360 test with QC20-W [640 x 360 pixels] [2.80 MB], [640 x 360 pixels] [7.69 MB]
|
|