|
22 results found.
|
RG4直线光栅 The RG4 open, non-contact optical linear encoder system eliminates friction and wear whilst permitting reliable high speed, high resolution operation. The 40 µm scale pitch allows higher speeds and greater set-up tolerances. In addition, RG4 systems are able to read a wider variety of scale types. [15 kB] Renishaw与超级巨无霸空客A380一起展翅高飞 Renishaw与超级巨无霸空客A380一起展翅高飞 网页内容 下载 致电当地的办事处 在线联系我们 事实上,无论从哪个方面衡量,在欧洲完成最终组装的最新超级巨无霸空客A380都是世界上最大的商用飞机。它能够搭载555名乘客,翼展宽达260英尺。建造这个双层巨无霸需要采用一些高度创新的装配技术。其中一项技术就是在几台机翼装配机上采用Renishaw的RG4直线光栅系统用于精确定位。四台装配机共使用了超过1公里的40微米栅距的钢带栅尺,用于移动‘轭’的精确定位。这些巨大的跨立式结构有4层楼高、80吨重,跨骑在每一个蒙皮壁板上,用于对整个翼展上的翼梁进行钻孔、攻丝及铆接。 创新系统... [15 kB] SiGNUM™直线光栅 High speed, non-contact performance, combined with dynamic signal processing and the IN-TRAC™ auto-phase optical reference mark. SiGNUM™ linear encoders are extremely easy to use yet offer a level of performance previously available only from more delicate fine pitch encoders. [20 kB] RG2和RG4增量式直线光栅 RG2和RG4增量式直线光栅 目前本页还没有简体中文版。您可以使用Google的翻译服务查阅 自动翻译 。我们不负责提供该项服务,而且翻译结果未经过我们的检查。 如果您需要更多帮助,请 联络我们 。 网页内容 下载 致电当地的办事处 在线联系我们 RG2 and RG4 products are the most commonly applied Renishaw encoders, providing highly-reliable position feedback, even in conditions considered unsuitable for most open... [11 kB] 光栅附件 To provide complete solutions for optical linear encoders and angle encoders a full range of accessories is available, for reference mark actuators to digital readouts. Renishaw is committed to providing position feedback solutions to satisfy customer specific requirements, such as custom angle encoder diameters and cross sections. [13 kB] 直线光栅 Renishaw提供品种繁多的高速直线光栅,能够满足工业自动化领域的不同需求。 [12 kB] RG2直线光栅 The RG2 is an open, non-contact optical linear encoder system, eliminating friction and wear whilst permitting reliable high speed, high resolution operation. The unique 20 µm pitch optics ensure excellent signal stability in conditions considered unsuitable for most open optical linear encoders. [17 kB] A380 panel assembly Inca Digital Printers has developed the first ever flatbed inkjet press, which looks set to revolutionise a major sector of the screen print market. Such hi-tech printing equipment demands advanced manufacturing techniques to ensure supreme accuracy, which in this case is provided by Renishaw RG2 encoders and assured by the use of the Renishaw ML10 laser calibration system, widely used across manufacturing industry. [15 kB] TONiC™直线光栅 TONiC™是Renishaw推出的新款超小型非接触式光栅,在直线光栅和圆光栅应用中均可达到10 m/s的速度和低至5 nm的分辨率。 TONiC™显著提高了Renishaw现有高速非接触式光栅的性能,改善了信号稳定性和长期可靠性,成本低,新颖的设计令人耳目一新。 [16 kB]
案例分析 — Renishaw与超级巨无霸空客A380一起展翅高飞 事实上,无论从哪个方面衡量,在欧洲完成最终组装的最新超级巨无霸空客A380都是世界上最大的商用飞机。它能够搭载555名乘客,翼展宽达260英尺。建造这个双层巨无霸需要采用一些高度创新的装配技术。其中一项技术就是在几台机翼装配机上采用Renishaw的RG4直线光栅系统用于精确定位。四台装配机共使用了超过1公里的40微米栅距的钢带栅尺,用于移动‘轭’的精确定位。这些巨大的跨立式结构有4层楼高、80吨重,跨骑在每一个蒙皮壁板上,用于对整个翼展上的翼梁进行钻孔、攻丝及铆接。 [33 kB] 案例分析 — Renishaw光栅尺促进微加工的研究 最近,一台特殊的设备由Ionoptika公司安装在了南安普顿大学,用于研究一项要求极高的应用:微加工。Renishaw就是这项研究中高度专业的供应商之一,为纳米运动所需的至关重要的定位提供RG2光栅尺和RGH25超高真空读数头。置身于这个学科之外的人们经常发现很难理解这样的工作是如何实现的 — 例如,Ionoptika的完整公司商标能够被蚀刻在一块典型的金属印网掩模上,而商标的宽度只有20 μm。 [37 kB]
|
|