|
301 results found.
|
XL-80系统软件 Software for use with Renishaw XL-80 system. Machine calibration and dynamic analysis. [11 kB] XL系统组件 The basis of the new system is a compact laser head (XL-80) and an independent environmental compensator system (XC-80). A tripod and stage may also be required depending upon the application. [15 kB] QuickViewXL™ QuickView XL is a software for use with Renishaw XL laser to give real time viewing and analysis of streaming laser measurement data. 50kHz capability. [11 kB] 效用 Tripods and cases assist with mounting and carrying your XL-80 laser system. The system cases are military specification, injection moulded plastic, with built-in wheels and handles. The new Universal tripod is smaller and lighter than previous options and benefits from a new armoured fabric case to make transporting the whole system easier. [13 kB] Renishaw宣布为HP5528和HP5529系统用户提供特殊升级组件 Renishaw宣布为HP5528和HP5529系统用户提供特殊升级组件 网页内容 下载 致电当地的办事处 在线联系我们 Renishaw的 XL-80 激光干涉仪系统自从2007年推出以来,取得了极大成功。该系统具有轻便、灵活、精确和使用方便的优点,是对机床、坐标测量机及其他位置精度至关重要的运动系统进行全面精度测量的理想工具。在当前经济形势尚不明朗的情况下,考虑到客户以往购买竞争厂商的设备已投入了大量资金,Renishaw宣布为现有HP用户专门推出了一套特殊升级组件。 Renishaw相信,XL... [16 kB] 校准服务商从更迅速、更智能化的工作中取得更多收益 Jürgen Emslander不是运动员,但他却能够以一步取胜,显著地提高自己的业绩,遥遥领先于同行。他经营了一家名为Geo Tec Messtechnik的校准服务公司,最近他将业界标准ML10激光校准系统升级为新型Renishaw XL-80系统。新系统的便携性和易用性极大地减少了运输和设定时间,增加了每个月的产能。 [20 kB] 升级与促销 There are many good reasons to buy the latest Renishaw measurement systems, and improve your business. [17 kB] ML10测量系统 自1988年推出以来,ML10激光测量系统(ML10激光干涉仪和EC10环境补偿单元)一直代表着机床、坐标测量机 (CMM) 及其他位置运动要求关键的系统精度校准的最高水准。 [13 kB] FASTRACK™直线光栅性能优势 FASTRACK™直线光栅性能优势 网页内容 下载 致电当地的办事处 在线联系我们 除了拥有硬化不锈钢结构的坚固性、安装便捷和栅尺拆卸/更换方便(即使在空间狭小受限的情况下也是如此)的优点外, FASTRACK 配用 RESOLUTE™ 和 TONiC™ 更能提供真正的性能优势! FASTRACK 光栅的安装 FASTRACK 简介 FASTRACK 绝对式光栅 FASTRACK 增量式光栅 高精度直线光栅 由于Renishaw的先进刻划工艺,用于 FASTRACK 的RTLC和RTLA栅尺具有±5 µm/m的给定精度,无需补偿。 更令人耳目一新的是,实际安装精度典型情况下接近于±2... [17 kB] 高速、可靠地印刷巨大图片 Like other technologies, it’s taken for granted. But, modern printing is a miracle of engineering precision, where producing a beautiful print is almost as complex as building a beautiful car. Thanks to Renishaw laser measurement technology, one company’s large-scale printers are considered the safe bet for consistency, reliability and stunning images. [19 kB] XL-80激光测量系统 新型Renishaw XL-80激光测量系统为坐标测量机和机床等运动系统提供高性能精度校准。 [14 kB] 质量 Many Renishaw users worldwide can testify to the performance and reliability in use of their Renishaw lasers and QC10 ballbars. The performance has been verified by national standards laboratories over many years and reliability is seen by users who find that systems operate ¢out of box¢ and continue to do so with minimal repairs over the years. [11 kB] 产品保修 产品保修 网页内容 下载 致电当地的办事处 在线联系我们 Renishaw的目标是提供满足或超出客户期望的产品和服务。购买测量和校准设备是您的一项重大投资,您对我们的产品和服务感到满意,这对我们的业务非常重要。 标准保修让您放心,相信Renishaw会免费修复产品的缺陷。 XL-80激光系统硬件的标准保修期为发货之日起3年。 QC10球杆仪系统硬件的标准保修期为发货之日起12个月。 后续步骤 如果您需要了解 更多信息 或者 询价 ,或有其他要求,可以直接联络 当地的Renishaw办事处 。 文档和下载 Calibration 全部 | 更多选项 联系Renishaw 全球分支机构... [8 kB] 光学镜组(附件) A number of optical accessories are available to ease set-up, alignment and operation of your ML10 laser system. [4 kB] 领先的光栅供应商将参加线性运动大师班 Renishaw, together with three other leading suppliers in the field of motion control, is supporting a linear motion conference organised by Eureka, a UK trade magazine for design engineers. The Linear Motion Masterclass is one of a series of the magazine’s ‘Design Days’, and takes place on 18th March 2008 at the Kaetsu Centre, Cambridge, UK. [16 kB]
新闻文章 - XL-80全新轻巧型激光干涉仪测量系统:便携性强、高性能、使用方便 你只要看一眼Renishaw的新型XL-80激光系统和XC-80补偿器,就会注意到它们比原有的ML10和EC10小了许多。现在,二者总重仅3公斤多一点(包括连接电缆、电源和传感器),比原来减轻了70%。当然,随着激光头和补偿器尺寸减小,其他系统组件,例如三脚架和云台也相应地减小以便相配,因此整个系统(配小型三脚架)的运输箱减小了许多。现在,最小的“脚轮箱”只有原来箱子的一半大一点,却可以携带整个线性和角度测量系统,并按需预留放置Renishaw QC10球杆仪组件的位置。这个高度便携的“检查和修正”激光干涉仪和球杆仪组合系统总重不到17公斤,令同类产品无以匹敌。 [48 kB] 新闻文章 - XL-80全新轻巧型激光干涉仪测量系统:便携性强、高性能、使用方便 你只要看一眼Renishaw的新型XL-80激光系统和XC-80补偿器,就会注意到它们比原有的ML10和EC10小了许多。现在,二者总重仅3公斤多一点(包括连接电缆、电源和传感器),比原来减轻了70%。当然,随着激光头和补偿器尺寸减小,其他系统组件,例如三脚架和云台也相应地减小以便相配,因此整个系统(配小型三脚架)的运输箱减小了许多。现在,最小的“脚轮箱”只有原来箱子的一半大一点,却可以携带整个线性和角度测量系统,并按需预留放置Renishaw QC10球杆仪组件的位置。这个高度便携的“检查和修正”激光干涉仪和球杆仪组合系统总重不到17公斤,令同类产品无以匹敌。 [361 kB]
XL80 in usePerson using an XL80 - [240 x 144 pixels] [35 kB]
- [450 x 270 pixels] [181 kB]
Laser XL software packagingLaserXL CD DVD case and cardboard sleeve - [100 x 106 pixels] [3 kB]
- [120 x 127 pixels] [4 kB]
- [160 x 170 pixels] [6 kB]
- [2440 x 2592 pixels] [2.41 MB]
Kompenzátor XC-80 a snímačeKompenzátor XC-80 je klíčovým prvkem pro zaručení přesnosti měření se systémem XL. - [140 x 119 pixels] [4 kB]
- [180 x 153 pixels] [6 kB]
- [1200 x 1022 pixels] [637 kB]
XL-80 SensorsXL-80 Sensors for accurate readings over a full range of operating conditions - [140 x 111 pixels] [4 kB]
- [540 x 429 pixels] [30 kB]
- [1200 x 953 pixels] [519 kB]
XL-80 calibration laser- [100 x 74 pixels] [2 kB]
- [140 x 103 pixels] [3 kB]
- [180 x 133 pixels] [4 kB]
- [1200 x 887 pixels] [677 kB]
XL-80 CMM 4XL-80 CMM 4 with laser and optics on granite table - [140 x 105 pixels] [4 kB]
- [720 x 540 pixels] [40 kB]
XL-80XL-80 Rear view - [140 x 84 pixels] [3 kB]
- [540 x 325 pixels] [24 kB]
XL-80XL-80 with laser - [100 x 81 pixels] [3 kB]
- [140 x 113 pixels] [6 kB]
- [1200 x 967 pixels] [833 kB]
Unità laser XL-80Sistema laser compatto XL-80 - [100 x 102 pixels] [3 kB]
- [140 x 143 pixels] [4 kB]
- [160 x 163 pixels] [5 kB]
- [180 x 183 pixels] [6 kB]
- [240 x 245 pixels] [8 kB]
- [540 x 550 pixels] [27 kB]
- [1861 x 1897 pixels] [849 kB]
XL-80 CMM 5- [180 x 151 pixels] [7 kB]
- [240 x 201 pixels] [12 kB]
- [522 x 438 pixels] [33 kB]
|
|